ContentPage

Bearing mounting tools

Bearings mounting guide:
methods and tools



Designed to withstand heavy loads and to extend the service life of machinery by reducing friction and distributing forces, bearings are very susceptible to shocks and heavy impacts. Therefore, improper handling or incorrect mounting and dismounting can damage the elements of a bearing, causing excessive noise and vibration levels, and affecting the bearing rotation.

The same can happen when small particles enter the bearing, causing the contamination of parts or of the lubricating substance. Even very small foreign particles can contaminate the bearing, jeopardizing the service life of the device. These types of bearing damage can be prevented by handling the devices properly and using the right tools when mounting and dismounting bearings.

ERIKS provides a comprehensive range of bearing tools intended to keep bearings well maintained during use, and to ensure the safe mounting and dismounting of bearings.

Full range of bearing tools

Wide assortment of bearing tools

Discover the full range of bearing tools in the ERIKS webshop and find the right product for your application.

View the range



Bearings mounting process


INSPECT ALL COMPONENTS FOR CONTAMINATION AND DAMAGE

Before mounting the bearings, make sure they are still in the original packages, to prevent contamination. Review the drawings to determine the correct orientation of the bearings in the assembly, and once you have everything ready, unpack the bearings and inspect them before mounting. If the bearings have been opened before and there’s a risk of contamination or damage, wash and dry them before mounting.

Check the area of the machine where the bearings will be mounted: this also needs to be clean, dry and dust-free. If you need to install housings, shafts or seals, make sure they are clean and dust-free. Check the lubrication holes and threaded holes for traces of substances from previous ensembles.

NOTE: New bearings may be covered in preservative. In most cases, it’s not necessary to wash this off, as long as you wipe off the outside and bore surfaces. However, it is necessary to double check if the lubricant you plan to use is compatible with the preservative. If not, you must wash and dry the bearing before mounting it. This doesn’t apply to bearings with seals and shields.

When all this is done, you can go to the second step of the process.

Wide range of bearing lubricants

Prevent bearing damage with the right lubricant

Discover the full range of bearing lubricants in the ERIKS webshop and find the right product for your application.

View the range



CHECK THE TOLERANCES OF ALL ELEMENTS IN THE ASSEMBLY

The dimensional and geometrical tolerances of the pieces in the assembly must be checked before starting the mounting, as the performance of bearings can be severely affected by poorly chosen associated components. The tolerances of bearings are described by tolerance classes, as defined in the ISO 492 (radial bearings) and ISO 199 (thrust bearings) standards. These classes are important as they influence the applications of bearings.

As you may know, a bearing’s tolerance refers to three aspects of accuracy: the external dimensional accuracy, the machining accuracy and the running accuracy. The dimensional accuracy gives the bearing’s external dimensions, such as bore diameter, outer diameter, inner ring width and outer ring width. This parameter is important for determining the shaft and housing fits in a bearing assembly.

The machining accuracy gives the precision of the manufacturing process and is important when choosing tolerances for shafts and housings. This parameter measures the variation in dimensions when comparing one bearing to another, for example inner and outer ring width variations.

The running accuracy or runout measures the radial runout and axial runout for the inner and outer ring, the side runout for the inner ring and the outer diameter runout for the outer ring. This parameter is important for minimizing vibration and misalignment in an assembly.

NOTE: For applications that require moderate rotation and operational speed, bearings with a Normal tolerance class are a good choice. However, for applications where more precision is needed, you should choose a bearing with a more accurate tolerance class. A tolerance Class 6 means less precision than a tolerance Class 4, and a Normal tolerance class is less precise than a Class 6. The tolerance class of the bearing should be chosen based on the application requirements for the previously mentioned parameters.

Since good bearing performance depends on adherence to the fits for the rings, the selection of the fits must be done before mounting the bearing. The rings should be well supported in the assembly, but not too tight, as depending on the application, the internal clearance of the bearing will change. Thus, the clearance should be adapted to the fits. This means that besides checking the tolerances, you should also make sure the bearing has the proper clearance and that the fits are not too loose or too tight.


Bearing mounting methods


Before starting to mount the bearings, make sure you wear the proper personal protection equipment for preventing injuries and product contamination. Safety gloves, shoes and goggles not only enhance workers’ safety, but also prevent the contamination of bearings with foreign particles.

PPE is especially important when handling hot or oily bearings, so make sure to check our guide on hand and arm protection if you need help in selecting the proper safety gloves for your company.

Safety gloves guide

Protect your hands when handling bearings

Read our Guide to hand and arm safety to learn about the different types of safety gloves in the ERIKS webshop, and choose the right product for your employees.

Read the guide



The choice for a mounting method depends on the bearing type and on the fits. Bearings with cylindrical bores are mounted in most cases by pressing them on the shafts, or by heating them, as this expands the diameter. Bearings with a tapered bore can be mounted directly on tapered shafts or cylindrical shafts using tapered sleeves.


MOUNTING BEARINGS WITH A CYLINDRICAL BORE

For bearings with cylindrical bore, the inner ring is mounted first. Still, if the bearing is non-separable, the tighter fit needs to be mounted first. If the ring is separable, then the inner ring will be mounted separately.

In both cases, the mounting can be done mechanically – and this procedure is called “cold mounting”, or by heating the bearing previous to mounting – and this procedure is referred to as “hot mounting”. A third method is hydraulic mounting, which is used mostly for large bearings.

For small bearings, meaning bearings with a diameter under 80 mm, both mechanical (cold) mounting and hot mounting can be used, but the preferred method is the mechanical or hydraulic press. For the press fitting method, a mounting tool is placed on the inner ring, then the bearing is pressed on the shaft, slowly, until the side of the inner ring rests against the shaft.

CAUTION: The pressing tool shouldn’t be placed on the outer ring, as this may damage the bearing. Before mounting, it’s recommended to apply oil on the shaft surface, to ensure a smooth insertion.

If no press is available, small bearings can also be mounted using a hammer and a mounting tool, such as a mounting sleeve with a flat face. This ensures an even distribution of the force over the entire ring circumference, reducing the risk of damaging the bearing.

This method is also preferred when the bearings require a tight fit, but should never be used for large bearings. The mounting tool should always be placed on the inner ring. For non-separable bearings that require a tight fit, the mounting tool is placed on both rings, and they are fitted at the same time with a hydraulic press, or with a screw.

Cold mounting of self-aligning bearings with cylindrical bore require the use of an intermediate mounting ring, which prevents the outer ring from moving when the device is introduced into the housing.

Bearings with a diameter of 80-200 mm are considered medium-sized, and those with a diameter larger than 200 mm are considered large. For both these categories, hot mounting is preferred. Hot mounting of bearings with a cylindrical bore applies to small bearings only when a very tight fit is needed. However, for large bearings, hot mounting is the preferred method.

Large bearings cannot usually be mounted without being heated as the force required to install them is very high. The temperature may vary depending on the type of bearing and manufacturer. For example, for SKF bearings the recommended heating temperatures are 80°C for capped bearings (with shields or seals), and 120°C for open bearings. For the hot mounting method, the risk of overheating the bearings locally is present, therefore SKF recommends using an electric induction heater for heating the devices evenly. With this method, the bearing is pre-heated, therefore the inner ring expands and is easier to install.

Other methods, such as heating the bearing in oil, can also be used, but in this case the risk of contamination increases. If hotplates are used, the bearings must be turned over several times, so it’s preferable to place a ring between the plate and the bearing to avoid damage. Also, if the bearings are capped, make sure the seals don’t come in direct contact with the plate.


MOUNTING BEARINGS WITH A TAPERED BORE

Bearings with a tapered bore are mounted on a tapered shaft or on a cylindrical shaft with an adapter or withdrawal sleeve. This is always done with an interference fit, the degree of interference being determined by how far the bearing is moved up onto a tapered shaft seat.

Small bearings with a bore diameter lower than 80 mm can be driven up onto the seat using a bearing fitting tool or a lock nut. For bearings mounted with an adapter sleeve, a hook or impact spanner should be used, and for those mounted with withdrawal sleeves, a bearing fitting tool or a nut are the best tools to use.

For medium-size bearings with a tapered bore, the proper bearing mounting tool is the impact spanner, but the drive-up method and the oil injection method can also be used. The last two techniques apply also to large-size bearings. For bearings with bore diameters greater than 200 mm, hydraulic nuts are recommended, and where applicable, SKF recommends using shafts and sleeves with grooves and ducts for the oil injection method.

The installation of large bearings using hydraulic nuts is applicable to tapered shaft seats, adapter sleeves and withdrawal sleeves. The hydraulic nut is positioned onto a threaded section of the shaft, or onto the thread of the sleeve, and rests on the inner ring of the bearing or on the shaft. When oil is pumped into the hydraulic nut, the piston is displaced axially thus the inner ring is driven up the taper, and mounted safely and accurately.

In the oil injection method (hydraulic method), also used for large bearings with tapered bore, oil under high pressure is injected via ducts and distribution grooves between the bearing and the seat. This oil forms a film between the two surfaces, which reduces friction, making mounting easier. Still, note that for this procedure, both the ducts and the grooves should already be in place, as part of the shaft design. If they aren’t, it is necessary to machine the oil grooves, feed channels and threaded connections into the shaft or sleeve before performing the oil injection.


BEARING MOUNTING METHODS OVERVIEW

Mechanical (cold) mounting Hot mounting Hydraulic mounting / oil injection
Bearing size Small, medium Small, medium, large Small, medium, large
Seat type Cylindrical, tapered, adapter sleeve, withdrawal sleeve Cylindrical Tapered, adapter sleeve, withdrawal sleeve
Tools used Fitting tool, hook spanner, impact spanner Hot plate induction heater, hot oil bath Hydraulic nut and pump, drive up method, oil injection method


Bearing mounting tools


You can use the selector below to quickly find the tools needed for mounting the bearings in your application. By clicking on the image or the tool name, you will be taken to the product page where you can easily add the tool in your cart.

Cylindrical
bore
Bore diameter Mechanical (cold) mounting Hot mounting Oil injection Hydraulic mounting
Small SKF bearing fitting tool
Fitting tool
Hot plate induction heater
Induction heater
Medium Hot plate induction heater
Induction heater
Large Induction heater
Induction heater
Tapered
bore
Small SKF hook spanner
Hook spanner
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Medium SKF impact spanner
Impact spanner
SKF oil injection kit
Oil injection kit
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Large SKF oil injection kit
Oil injection kit
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Adapter
sleeve
Small SKF hook spanner
Hook spanner
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Medium SKF impact spanner
Impact spanner
SKF oil injection kit
Oil injection kit
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Large SKF oil injection kit
Oil injection kit
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Withdrawal
sleeve
Small SKF bearing fitting tool
Fitting tool
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Medium SKF oil injection kit
Oil injection kit
SKF hydraulic pump
Hydraulic pump for
Drive-up method
Large SKF oil injection kit
Oil injection kit
SKF hydraulic pump
Hydraulic pump for
Drive-up method


Do you have questions about our products?
For personal advise and product knowledge, visit an ERIKS location near you or contact our product specialists.

Find a service center | Call us | Send us an e-mail



CONTENTS
1. Bearings mounting process
1.1 Inspection
1.2 Checking tolerances
2. Bearing mounting methods
2.1 Bearings with cylindrical bore
2.2 Bearings with tapered bore
2.3 Mounting methods overview
3. Bearing mounting tools

Subscribe to the ERIKS newsletter

Thank you for subscribing!

Fill in your e-mail address

Subscribing to the newsletter has failed