CategoryPage

Taper Roller Bearings Imperial (18 products containing 8169 Items)


Grid    
List    
1 / 2
Next
Grid    
List    
1 / 2
Next

Imperial tapered bearings have inner and outer ring races between the rollers. The projection lines of the surfaces hit each other at the same point on the shaft. This design makes it possible to absorb radial and axial loads simultaneously.


The contact angle largely determines the axial load capacity of the bearings. The greater the angle, the higher the axial load capacity. The logarithmic contact profile ensures optimum distribution of stress on the roller contact. Due to the special design of the surfaces of the flange and the large roller, the lubricant is guided into the roller better. The benefits of this are the increased operational reliability and reduced sensitivity to misalignment. Imperial tapered bearings are often used in sets. Imperial tapered bearings are the most commonly used bearings in the wheel bearing ring. For example, all commercial aircraft take off and land using wheels mounted on tapered bearings.