CategoryPage

Lubricants (0 products containing 0 Items)


Grid    
List    
1 / 0
Grid    
List    
1 / 0

Lubricants are an important part of bearings. A lubricant reduces friction and ensures that there is less wear, as a result of which the bearing has a longer service life. Friction is the force created by two surfaces moving against each other. Wear is a change in the surface as a result of the removal of abrasive deposits due to mechanical contact. Wear also occurs as a result of the heat generated by friction.


There are many types of lubricants that can be used for a wide range of applications. The lubricants in the webshop are products from the top brands that have been specially selected by lubrication experts to ensure that the lubricants are of good quality with proven performance.